Tool/software:
Part-1 (capacitance connection)
Can a common 10 uF capacitance be used for pins 25,41 and 57 (VCC Mash, VCCVCO2 and VCCVCO respectively),
or should they be individually terminated using 10uF capacitance each.
If a common capacitance is used what can be the consequences.
Part -2 (resistive termination)
Data sheet recommends termination of parallel pin control pins (3, 4, 15, 16, 17, 18, 19, and 20) by 1 Kohm resistance.
What is the use of this termination and why 1Kohm, can it be terminated by 1.8Kohm resistor.