I use the CDCE62005 (LVPECL mode) to drive a HCSL CLK input.
I've used the interface as described in the CDCM61001 datasheet, page 26 (http://www.ti.com/lit/ds/symlink/cdcm61001.pdf)
On the output, I see an AM modulated signal with a high frequency of 100MHz (wanted) and a low frequency of 7.5 KHz. The amplitude varies between 400 mV-pp and
1.2 V-pp (single-ended). This effect is visible with a single-ended and differential probe.
What is possibly the reason of the variation in amplitude? All other LVDS outputs works fine.
I remove the two 150R resistors to GND, place a 100R termination resistor on both lines (such as LVDS termination), and the signal output is fine.
But does this type of termination reduce the reliability of the CDCE62005?
Thanks in advance
Jacob