Part Number: LMX2572
Other Parts Discussed in Thread: LMX2592
Tool/software:
Dear Team,
My customer has evaluated the LMX2572.
As a continuing challenge, the lock time of the PLL has become an issue.
The following are the issues they are considering.
・ LMX2572
- FOSC: 40.96 MHz with partial assist -> VCOcal is 98us
Measures against measurement variation when implemented in their Measurement Instruments (spurious of PLL Output Signal?) as
Kpd: 0.625mA, MASH Order: 4th
They want this to be less than 100us including the lock time without Full Assist.
・ Changed Fosc
- Fosc: 81.92MHz with Partial Assist -> Total 108.3us
Mash Order: 3rd Loop Gain Change error with FVCO less than 3604.5GHz (resolved in Kpd 1.25mA)
・ Fast calibration on LMX2592
- Fosc: 40.96 MHz VCOcal30us Total: 90.9us
If tjey have the same loop filter and same Kpd as LMX2572, they get Loop Gain Change error
They are considering this.
Could you give me some advice?
As for Full Assist, they would like to achieve PLL lock time < 100us without using Full Assist if possible.
Because;
- To be used as a measuring signal for measuring instruments.
- This is because they don't know everything about the problems of giving a fixed assist value at their factory.
They think;
- The value changes as the temperature changes.
- It also depends on the individual differences of chips.
And so on.
Therefore, they want to turn on and use VCOcal itself.
Best Regards,
Koshi Ninomiya