Part Number: CDCDB800
Other Parts Discussed in Thread: DS320PR1601, LMKDB1108
Tool/software:
Hi,
We are using CDCDB800 clock buffer along with DS320PR1601, in the said clock buffer's datasheet it is mentioned that default termination is 85ohm.
But we are using PCIe Gen 5 Refclk having 100ohm differential impedance.
In clock buffer's datasheet it is specified that we can change the impedance from 85ohm to 100ohm(OUTSET register, bit5).
In section 6.5(Electrical characterstics) it is specified that Zdiff by default is 85ohm but it can be set to 100ohm by setting the respective bit to 1 in OUTSET register.
But this has to be programmed each time when we turn ON the unit, which is practically impossible.
How can we overcome this scenario?
Thanks and Regards,
Shekha Shoukath