Part Number: CDCM7005
Other Parts Discussed in Thread: CDCE62005
Tool/software:
I would like to ask if it is possible to output 24.32MHz ~ 26.88MHz when the Ref Clock Input Range is 380KHz ~ 420KHz using CDCM7005.
The output clock is Ref clock * 64
And using CDCM7005, another frequency usage is when the Ref Clock input range is 12MHz ~ 15MHz, can Output clock 1 output 98.8MHz ~ 109.2MHz and Output clock 2 output 197.6MHz ~ 218.4MHz
That is, Output clock 1 output clock is Ref clock * 8. And Output clock 2 output clock is Ref clock * 16