Part Number: LMK05318B-Q1
Other Parts Discussed in Thread: LMK05318B, LMK5B12204
Tool/software:
I had this working with my LMK12204s but for the life of me, I can't get it to work with the LMK05318B-Q1s.
I'm seeing really odd behavior. The configs I've attached exhibit the following behavior...
When the registers are written live, I can issue a RESET_SW and the outputs will mute and less than a second later turn on locked to the input but not synced. I can RESET_SW multiple times with the same result.
If I then issue a SYNC_SW command, the outputs will stay on but the DPLL will unlock for both phase and frequency and stay that way until I issue another RESET_SW.
Now if that's not strange enough, if I export the EEPROM map without changing anything in TICSPro, write the EEPROM, then do a PDN, the outputs come up unmuted and the DPLL unlocked. I then have to do a RESET_SW to get them back but they're still unsynced.
At one point during my fiddling, I got into a situation where after a RESET_SW the outputs would mute, then come back almost-synced BUT NOT LOCKED TO THE INPUT. A SYNC_SW would then sync them but they'd stay unlocked.
I've been running around in circles for 2 days now trying various combinations of options. Even the exact options I used for the 12204s don't do the same thing on the 05318Bs.
Any help would be appreciated
.lmk05-10mhz-rev8-sync-mute.tcs
R0 0x000010 R1 0x00010B R2 0x000235 R3 0x000332 R4 0x000404 R5 0x00050E R6 0x000617 R7 0x00078E R8 0x000802 R10 0x000AC8 R11 0x000B00 R12 0x000C1B R13 0x000D08 R14 0x000E00 R15 0x000F00 R16 0x001000 R17 0x00111D R18 0x0012FF R19 0x001308 R20 0x001420 R21 0x001501 R22 0x001600 R23 0x001755 R24 0x0018FF R25 0x0019F0 R26 0x001A00 R27 0x001B00 R28 0x001C01 R29 0x001D03 R30 0x001E40 R32 0x002044 R35 0x002300 R36 0x002403 R37 0x002500 R38 0x002600 R39 0x002702 R40 0x00280F R41 0x002900 R42 0x002A11 R43 0x002BC2 R44 0x002C00 R45 0x002D0C R46 0x002E88 R47 0x002F07 R48 0x003050 R49 0x00314A R50 0x003200 R51 0x003300 R52 0x003400 R53 0x0035F9 R54 0x003600 R55 0x003700 R56 0x0038F9 R57 0x00393F R58 0x003AF9 R59 0x003B3F R60 0x003CF9 R61 0x003D3F R62 0x003EF9 R63 0x003F3F R64 0x004000 R65 0x004100 R66 0x004200 R67 0x0043F9 R68 0x004408 R69 0x004500 R70 0x004601 R71 0x004700 R72 0x004833 R73 0x004900 R74 0x004A00 R75 0x004B00 R76 0x004C00 R77 0x004D0F R78 0x004E00 R79 0x004F11 R80 0x005080 R81 0x00510A R82 0x005200 R83 0x005307 R84 0x005480 R85 0x005500 R86 0x005600 R87 0x00571E R88 0x005884 R89 0x005980 R90 0x005A00 R91 0x005B14 R92 0x005C00 R93 0x005D07 R94 0x005E80 R95 0x005F00 R96 0x006000 R97 0x00611E R98 0x006284 R99 0x006380 R100 0x006429 R101 0x006501 R102 0x006622 R103 0x00670F R104 0x00681F R105 0x006905 R106 0x006A00 R107 0x006B64 R108 0x006C00 R109 0x006D61 R110 0x006EA8 R111 0x006F00 R112 0x007000 R113 0x007100 R114 0x007200 R115 0x007303 R116 0x007401 R117 0x007500 R118 0x007600 R119 0x007700 R120 0x007800 R121 0x007900 R122 0x007A00 R123 0x007B28 R124 0x007C00 R125 0x007D11 R126 0x007E79 R127 0x007F7A R128 0x008000 R129 0x008101 R130 0x008200 R131 0x008301 R132 0x008401 R133 0x008577 R134 0x008600 R135 0x00872B R136 0x008800 R137 0x008928 R138 0x008AE5 R139 0x008B03 R140 0x008C02 R141 0x008D00 R142 0x008E01 R143 0x008F01 R144 0x009077 R145 0x009101 R146 0x009289 R147 0x009320 R149 0x00950D R150 0x009600 R151 0x009701 R152 0x00980D R153 0x009929 R154 0x009A24 R155 0x009B32 R156 0x009C01 R157 0x009D00 R158 0x009E00 R159 0x009F00 R160 0x00A0FC R161 0x00A132 R162 0x00A200 R164 0x00A400 R165 0x00A500 R167 0x00A701 R178 0x00B200 R180 0x00B400 R181 0x00B500 R182 0x00B600 R183 0x00B700 R184 0x00B800 R185 0x00B905 R186 0x00BA08 R187 0x00BB00 R188 0x00BC00 R189 0x00BD00 R190 0x00BE98 R191 0x00BF00 R192 0x00C0F0 R193 0x00C12F R194 0x00C22F R195 0x00C300 R196 0x00C400 R197 0x00C544 R198 0x00C600 R199 0x00C700 R200 0x00C844 R201 0x00C900 R202 0x00CA00 R203 0x00CB00 R204 0x00CC38 R205 0x00CD00 R206 0x00CE00 R207 0x00CF38 R208 0x00D000 R209 0x00D114 R210 0x00D200 R211 0x00D316 R212 0x00D400 R213 0x00D528 R214 0x00D600 R215 0x00D72C R216 0x00D80F R217 0x00D900 R218 0x00DA00 R219 0x00DB13 R220 0x00DC13 R221 0x00DD00 R222 0x00DE03 R223 0x00DF0D R224 0x00E048 R225 0x00E100 R226 0x00E200 R227 0x00E326 R228 0x00E426 R229 0x00E500 R230 0x00E606 R231 0x00E71A R232 0x00E88F R233 0x00E90B R234 0x00EA0B R235 0x00EB00 R236 0x00ECC3 R237 0x00ED50 R238 0x00EE00 R239 0x00EF00 R240 0x00F0C3 R241 0x00F150 R242 0x00F200 R243 0x00F300 R244 0x00F400 R249 0x00F921 R250 0x00FA00 R251 0x00FB23 R252 0x00FC2D R253 0x00FD00 R254 0x00FE00 R255 0x00FF00 R256 0x010000 R257 0x010101 R258 0x010200 R259 0x010301 R260 0x010402 R261 0x010580 R262 0x010600 R263 0x010700 R264 0x010800 R265 0x010901 R266 0x010AF4 R267 0x010BA0 R268 0x010C0C R269 0x010D03 R270 0x010E02 R271 0x010FB6 R272 0x011000 R273 0x011100 R274 0x011200 R275 0x01130E R276 0x01140C R277 0x01150E R278 0x011609 R279 0x011708 R280 0x011809 R281 0x011907 R282 0x011A0D R283 0x011B07 R284 0x011C1E R285 0x011D1E R286 0x011E02 R287 0x011F70 R288 0x012003 R289 0x0121EC R290 0x012203 R291 0x01230A R292 0x012409 R293 0x012501 R294 0x012600 R295 0x01272C R296 0x012806 R297 0x01290A R298 0x012A06 R299 0x012B01 R300 0x012C00 R301 0x012D1C R302 0x012E20 R303 0x012F01 R304 0x013000 R305 0x013100 R306 0x013200 R307 0x013300 R308 0x01343E R309 0x013580 R310 0x013600 R311 0x013700 R312 0x013800 R313 0x013900 R314 0x013A00 R315 0x013B00 R316 0x013C00 R317 0x013D00 R318 0x013E00 R319 0x013F03 R320 0x014000 R321 0x01410A R322 0x014200 R323 0x01430E R324 0x0144A6 R325 0x014500 R326 0x014600 R327 0x014798 R328 0x014896 R329 0x014980 R330 0x014A00 R331 0x014B64 R332 0x014C00 R333 0x014D00 R334 0x014E3D R335 0x014F09 R336 0x015000 R337 0x015198 R338 0x015296 R339 0x015380 R340 0x015400 R341 0x015500 R342 0x015600 R343 0x015700 R344 0x015800 R345 0x015900 R346 0x015A02 R347 0x015B00 R348 0x015C00 R349 0x015D00 R350 0x015E00 R351 0x015F00 R352 0x016000 R357 0x016528 R367 0x016F00 R411 0x019B0C
[EEPROM_IMAGE] COUNT=253 DATE_TIME=2025-07-02, 15:56:07 EEPROM_IMG_IDX00=4 EEPROM_IMG_IDX01=14 EEPROM_IMG_IDX02=23 EEPROM_IMG_IDX03=142 EEPROM_IMG_IDX04=50 EEPROM_IMG_IDX05=1 EEPROM_IMG_IDX06=137 EEPROM_IMG_IDX07=32 EEPROM_IMG_IDX08=0 EEPROM_IMG_IDX09=100 EEPROM_IMG_IDX10=200 EEPROM_IMG_IDX11=0 EEPROM_IMG_IDX12=120 EEPROM_IMG_IDX13=0 EEPROM_IMG_IDX14=127 EEPROM_IMG_IDX15=250 EEPROM_IMG_IDX16=42 EEPROM_IMG_IDX17=255 EEPROM_IMG_IDX18=248 EEPROM_IMG_IDX19=0 EEPROM_IMG_IDX20=0 EEPROM_IMG_IDX21=33 EEPROM_IMG_IDX22=208 EEPROM_IMG_IDX23=13 EEPROM_IMG_IDX24=41 EEPROM_IMG_IDX25=240 EEPROM_IMG_IDX26=53 EEPROM_IMG_IDX27=32 EEPROM_IMG_IDX28=6 EEPROM_IMG_IDX29=2 EEPROM_IMG_IDX30=15 EEPROM_IMG_IDX31=0 EEPROM_IMG_IDX32=156 EEPROM_IMG_IDX33=32 EEPROM_IMG_IDX34=50 EEPROM_IMG_IDX35=32 EEPROM_IMG_IDX36=61 EEPROM_IMG_IDX37=9 EEPROM_IMG_IDX38=64 EEPROM_IMG_IDX39=0 EEPROM_IMG_IDX40=0 EEPROM_IMG_IDX41=249 EEPROM_IMG_IDX42=0 EEPROM_IMG_IDX43=3 EEPROM_IMG_IDX44=228 EEPROM_IMG_IDX45=255 EEPROM_IMG_IDX46=228 EEPROM_IMG_IDX47=255 EEPROM_IMG_IDX48=228 EEPROM_IMG_IDX49=255 EEPROM_IMG_IDX50=228 EEPROM_IMG_IDX51=252 EEPROM_IMG_IDX52=0 EEPROM_IMG_IDX53=0 EEPROM_IMG_IDX54=3 EEPROM_IMG_IDX55=228 EEPROM_IMG_IDX56=32 EEPROM_IMG_IDX57=0 EEPROM_IMG_IDX58=0 EEPROM_IMG_IDX59=3 EEPROM_IMG_IDX60=192 EEPROM_IMG_IDX61=17 EEPROM_IMG_IDX62=0 EEPROM_IMG_IDX63=20 EEPROM_IMG_IDX64=0 EEPROM_IMG_IDX65=60 EEPROM_IMG_IDX66=0 EEPROM_IMG_IDX67=0 EEPROM_IMG_IDX68=3 EEPROM_IMG_IDX69=208 EEPROM_IMG_IDX70=144 EEPROM_IMG_IDX71=0 EEPROM_IMG_IDX72=5 EEPROM_IMG_IDX73=0 EEPROM_IMG_IDX74=7 EEPROM_IMG_IDX75=128 EEPROM_IMG_IDX76=0 EEPROM_IMG_IDX77=0 EEPROM_IMG_IDX78=122 EEPROM_IMG_IDX79=18 EEPROM_IMG_IDX80=0 EEPROM_IMG_IDX81=164 EEPROM_IMG_IDX82=165 EEPROM_IMG_IDX83=239 EEPROM_IMG_IDX84=148 EEPROM_IMG_IDX85=25 EEPROM_IMG_IDX86=1 EEPROM_IMG_IDX87=134 EEPROM_IMG_IDX88=160 EEPROM_IMG_IDX89=0 EEPROM_IMG_IDX90=0 EEPROM_IMG_IDX91=0 EEPROM_IMG_IDX92=0 EEPROM_IMG_IDX93=12 EEPROM_IMG_IDX94=128 EEPROM_IMG_IDX95=0 EEPROM_IMG_IDX96=0 EEPROM_IMG_IDX97=0 EEPROM_IMG_IDX98=0 EEPROM_IMG_IDX99=8 EEPROM_IMG_IDX100=4 EEPROM_IMG_IDX101=31 EEPROM_IMG_IDX102=197 EEPROM_IMG_IDX103=96 EEPROM_IMG_IDX104=5 EEPROM_IMG_IDX105=28 EEPROM_IMG_IDX106=160 EEPROM_IMG_IDX107=97 EEPROM_IMG_IDX108=0 EEPROM_IMG_IDX109=65 EEPROM_IMG_IDX110=252 EEPROM_IMG_IDX111=0 EEPROM_IMG_IDX112=0 EEPROM_IMG_IDX113=0 EEPROM_IMG_IDX114=0 EEPROM_IMG_IDX115=0 EEPROM_IMG_IDX116=208 EEPROM_IMG_IDX117=0 EEPROM_IMG_IDX118=0 EEPROM_IMG_IDX119=2 EEPROM_IMG_IDX120=96 EEPROM_IMG_IDX121=190 EEPROM_IMG_IDX122=240 EEPROM_IMG_IDX123=0 EEPROM_IMG_IDX124=17 EEPROM_IMG_IDX125=0 EEPROM_IMG_IDX126=0 EEPROM_IMG_IDX127=68 EEPROM_IMG_IDX128=0 EEPROM_IMG_IDX129=0 EEPROM_IMG_IDX130=56 EEPROM_IMG_IDX131=0 EEPROM_IMG_IDX132=0 EEPROM_IMG_IDX133=224 EEPROM_IMG_IDX134=0 EEPROM_IMG_IDX135=160 EEPROM_IMG_IDX136=1 EEPROM_IMG_IDX137=96 EEPROM_IMG_IDX138=5 EEPROM_IMG_IDX139=0 EEPROM_IMG_IDX140=11 EEPROM_IMG_IDX141=60 EEPROM_IMG_IDX142=0 EEPROM_IMG_IDX143=4 EEPROM_IMG_IDX144=196 EEPROM_IMG_IDX145=192 EEPROM_IMG_IDX146=12 EEPROM_IMG_IDX147=53 EEPROM_IMG_IDX148=32 EEPROM_IMG_IDX149=0 EEPROM_IMG_IDX150=9 EEPROM_IMG_IDX151=137 EEPROM_IMG_IDX152=128 EEPROM_IMG_IDX153=24 EEPROM_IMG_IDX154=106 EEPROM_IMG_IDX155=61 EEPROM_IMG_IDX156=107 EEPROM_IMG_IDX157=1 EEPROM_IMG_IDX158=134 EEPROM_IMG_IDX159=160 EEPROM_IMG_IDX160=0 EEPROM_IMG_IDX161=3 EEPROM_IMG_IDX162=13 EEPROM_IMG_IDX163=64 EEPROM_IMG_IDX164=0 EEPROM_IMG_IDX165=0 EEPROM_IMG_IDX166=8 EEPROM_IMG_IDX167=66 EEPROM_IMG_IDX168=203 EEPROM_IMG_IDX169=128 EEPROM_IMG_IDX170=0 EEPROM_IMG_IDX171=0 EEPROM_IMG_IDX172=0 EEPROM_IMG_IDX173=128 EEPROM_IMG_IDX174=0 EEPROM_IMG_IDX175=40 EEPROM_IMG_IDX176=0 EEPROM_IMG_IDX177=0 EEPROM_IMG_IDX178=0 EEPROM_IMG_IDX179=62 EEPROM_IMG_IDX180=148 EEPROM_IMG_IDX181=48 EEPROM_IMG_IDX182=117 EEPROM_IMG_IDX183=176 EEPROM_IMG_IDX184=0 EEPROM_IMG_IDX185=0 EEPROM_IMG_IDX186=230 EEPROM_IMG_IDX187=57 EEPROM_IMG_IDX188=40 EEPROM_IMG_IDX189=73 EEPROM_IMG_IDX190=218 EEPROM_IMG_IDX191=127 EEPROM_IMG_IDX192=122 EEPROM_IMG_IDX193=112 EEPROM_IMG_IDX194=251 EEPROM_IMG_IDX195=48 EEPROM_IMG_IDX196=169 EEPROM_IMG_IDX197=66 EEPROM_IMG_IDX198=193 EEPROM_IMG_IDX199=138 EEPROM_IMG_IDX200=25 EEPROM_IMG_IDX201=3 EEPROM_IMG_IDX202=144 EEPROM_IMG_IDX203=2 EEPROM_IMG_IDX204=0 EEPROM_IMG_IDX205=0 EEPROM_IMG_IDX206=0 EEPROM_IMG_IDX207=31 EEPROM_IMG_IDX208=64 EEPROM_IMG_IDX209=0 EEPROM_IMG_IDX210=0 EEPROM_IMG_IDX211=0 EEPROM_IMG_IDX212=0 EEPROM_IMG_IDX213=0 EEPROM_IMG_IDX214=0 EEPROM_IMG_IDX215=0 EEPROM_IMG_IDX216=0 EEPROM_IMG_IDX217=0 EEPROM_IMG_IDX218=3 EEPROM_IMG_IDX219=0 EEPROM_IMG_IDX220=20 EEPROM_IMG_IDX221=0 EEPROM_IMG_IDX222=117 EEPROM_IMG_IDX223=48 EEPROM_IMG_IDX224=0 EEPROM_IMG_IDX225=19 EEPROM_IMG_IDX226=18 EEPROM_IMG_IDX227=208 EEPROM_IMG_IDX228=0 EEPROM_IMG_IDX229=25 EEPROM_IMG_IDX230=0 EEPROM_IMG_IDX231=0 EEPROM_IMG_IDX232=61 EEPROM_IMG_IDX233=9 EEPROM_IMG_IDX234=2 EEPROM_IMG_IDX235=98 EEPROM_IMG_IDX236=90 EEPROM_IMG_IDX237=0 EEPROM_IMG_IDX238=0 EEPROM_IMG_IDX239=0 EEPROM_IMG_IDX240=0 EEPROM_IMG_IDX241=0 EEPROM_IMG_IDX242=0 EEPROM_IMG_IDX243=16 EEPROM_IMG_IDX244=0 EEPROM_IMG_IDX245=0 EEPROM_IMG_IDX246=0 EEPROM_IMG_IDX247=0 EEPROM_IMG_IDX248=0 [META] DEVICE=LMK05318B DATA=SRAM WORD_SIZE_BITS=24 RAMDAT_ADDR=R162[7:0] MEMDAT_ADDR=R159[4:0], R159[7:0] PART_ID_ADDR=R3[7:0], R2[7:0] PART_ID_VALUE=0x1135 [FREQUENCY] XO=12800000