This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5C33216EVM: not able to create an output signal

Part Number: LMK5C33216EVM
Other Parts Discussed in Thread: LMK5C33216A

Tool/software:

We are using a board LMK5C33216EVM in our development process and TICSPro. The board is running, and SPI communication is working. However, I'm currently not able to create any output signal. Regardless of the loaded configuration/registers, the scope is always showing only 125MHz on OU0 and 156.25MHz on OUT1. I have read manuals from the website, and also tried to load multiple config files from TI forum, bt the result is always the same.
In the first step, the board should produce output signals of different frequencies, just as a test. In the next step, it should accept a signal (frequency or PPS) and reproduce the same output, shifted for unesenu vrijednost (in ns or ps).
Any help would be appreciated.

on behalf of my customer
Thanks and bye 
Hanno