Tool/software:
Hi Community
I am currently making some experiments with the EVM Kit and have some questions about the STATUS flags.
My setup is configured as follow : PRIREF=10MHz ; XO=32.768 MHZ ; DPLL used with 30 Hz bandwidth ; PLL2 unused.
I am also using the LEds indicators to monitor status flags in real time. (R48 register making the selection). specially PLL1 behaviour
- What is the PLL1 Digital lock detect (mentionned in the datasheet but without explanation) compared to APLL1_lock_detect ?
- For example selecting "PLL1 DLD makes" the status led to bright , while selecting "APLL1_lock_detect" switches OFF the LED
- When selecting "APLL1_lock_detect" the led is always OFF independently of PRIREF being active or not .
- idem for PLL1 DLD which is always ON
with best regards,
Bruno