This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL5010: TPL5010 not generating wake pulse

Part Number: TPL5010


Tool/software:

I am using the TPL5010 in a new design the wake drives an interrupt in the CPU and the CPU responds with DONE. For some reason the wake pulse does not seem to be happening. Every 90 minutes as set by the timing resistor the system resets, as it should. When I attached a cro probe to the wake pin I see the wake pulse and I can see the done response and the system works. If I remove the cro the system does not work. what is the output drive circuit from the TPL5010? I tried a pull down resistor on the cpu input pin, no improvement. Any suggestions appreciated.