This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMKDB1120: LMKDB1120Z85NPPR spec question

Part Number: LMKDB1120

Tool/software:

Hi E2E,

Could you kindly help to check the question from customer as below? I also loop customer in.

What is the function of this pin? And what situation we need to enable it.

BR,

Janet

  • Hello Janet, 
    This is "Loss of Signal". 
    This pin is high when a valid input clock is present or goes low when the input is lost. 
    You use this pin in any situation where you need to determine if the clock is valid. This could go to your FPGA or MCU for monitoring to see if the line ever goes low. 
    Or you can just it as a visual indicator - with an LED. 

    Best regards, 

    Vicente