Part Number: LMX2615-SP
Tool/software:
Hi,
I am using LMX2615 for clocking the RF DAC.So I am configuring LMX2615 in the "TICS pro"
In TICS Pro,I need to give 187.5MHz as FOSC and need to generate 12GHz from RFOutA and also need to generate SYSREF in the Second Channel (RFOutB).
While I selecting the SYSREF for 2nd channel,By default I need to enable the "SYSREF_EN" and "VCO_PHASE_SYNC".So If I enable the "VCO_PHASE_SYNC",the N divider is limited above 29.
Kindly suggest the solution to give above mentioned frequency and why the N divider value is limited?