This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214-Q1: CDCE6214-Q1

Part Number: CDCE6214-Q1

Tool/software:

Do you have a similar part that rated to 125C for automotive usage? CDCE6214-Q1 is only rated to 105C. Thank you.

  • My question is can we use the increment/decrement pins to do 0.03ppm (or better) step size from 90MHz to 100MHz output.

    Output glitches are not acceptable

    I only need one LVDS output.

    125C would be nice.

    Very small package size is desired.

  • Wilbur,

    Will your application require temperatures up to 125C ambient?

    If the junction temperature is below 125C, then the CDCE6214-Q1 can be used. The power consumption of the device is fairly low (~50mA typical for four outputs operating), meaning that, for your application, temperatures above 105C can be achieved (especially when using a 1.8V supply) before hitting 125C junction temperature.

    Otherwise, we do not have a device with this functionality that supports 125C ambient temperature.

    Thanks,

    Kadeem

  • Kadeem,

    I will have one  100MHz LVDS output, so my power dissipation should be on the low side.

    Thank you for the feedback.