Part Number: TICSPRO-SW
Other Parts Discussed in Thread: USB2ANY, LMK05318B, LMK5B12204
Tool/software:
TICS Pro v1.7.9.0
* When TICS Pro starts with a USB2ANY connected, it writes registers R68, R202, R203, R204, R205, R206, R207 to the device. Should it really be writing registers to a device before it's even loaded a tcs file? And why those registers specifically?
Welcome to TICS Pro. Version -> 1.7.9.0, 27-May-25
Loading Device LMK05318B...
Detected 1 USB2ANY interfaces
Wrote Register R68 (0x44) as 0x00 4408
Wrote Register R68 (0x44) as 0x00 4408
Wrote Register R202 (0xCA) as 0x00 CA00
Wrote Register R203 (0xCB) as 0x00 CB00
Wrote Register R204 (0xCC) as 0x00 CC38
Wrote Register R68 (0x44) as 0x00 4408
Wrote Register R68 (0x44) as 0x00 4408
Wrote Register R205 (0xCD) as 0x00 CD00
Wrote Register R206 (0xCE) as 0x00 CE00
Wrote Register R207 (0xCF) as 0x00 CF38
Completed loading Device LMK05318B. Version = 2025-05-06, v0.12.8
* TICS Pro doesn't seem to save the AutoUpdate option.
* When TICS Pro loads a tcs file with a USB2ANY connected it automatically writes all registers it to the device which I don't think is a good idea, especially if AutoUpdate is off. It also writes it even if the device in the tcs file doesn't match the device connected. I.E if you have a LMK05318B connected and load a LMK5B12204 tcs file to use as a base, TICS Pro still writes all the registers. Also not a good idea.
* It also writes all registers if you select one of the default configurations even if AutoUpdate is off. This really isn't a good idea.
* On the Wizard Set Reference page, If you change the value of PRIREF frequency it often resets the interface type to AC, hysteresis = 200mv