Hi,
I have used the CDCE72010 GUI app to set up one of these devices on another board and have done so successfully.
I've exported the register state I like from the GUI and used it to program another CDCE72010 in another system, but I don not get any output clocks after doing so.
The 1st system has a TUSB3210 USB port I access through the GUI.
The 2nd system I am using an Aardvark USB/SPI dongle.
I have captured the SPI data streams being written to both systems with a logic analyzer and verified they are in fact identical.
What am I missing that would prevent the chip in the 2nd system from outputting clocks? I tried a reset but that doesn't seem to make any difference.
The one difference between the 2 systems is the 1st is driven by an LVCMOS level clock and the 2nd is driven by LVDS. (I did change the VCXO input to LVDS, external termination, DC)
By the way, why does this chip want SPI data LSB first? That's a pain. I have to take all the data from the GUI, mirror it and then re-enter the result in my SPI tool. :-(
Plug: Excalibur free calculator for Windows does a nice job with that. http://home.comcast.net/~dbernazzani/
Thanks.