Part Number: LMX2572
Tool/software:
Is it Possible to achieve
Frequency sweep 1 (in Ramp Up-Down configuration):
Start: 2.4 GHz
Stop: 2.485 GHz
Sweep time/sweep rate: 0.1 μs/ 10 MHz
Frequency sweep 2 (in Ramp Up-Down configuration):
Start: 5.725 GHz
Stop: 5.85 GHz
Sweep time/sweep rate: 0.1 μs/ 10 MHz
If not achievable Provide us with alternative methods with which i will be able to achieve in detail.
And what is the Minimum Time period with which i can sweep the 150MHz band.
If i disable the Vco Calibration will it effect my Ramp Signal Drastically.