Part Number: LMK3H0102
Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hi Support Team,
I am using the LMK3H0102A016RERR, and its output is 50 MHz.
However, my actual requirement is 100 MHz.
Therefore, I would like to adjust the output frequency through I²C.
I referred to the datasheet and followed the steps below, but I did not get any output. Could you please help me confirm if there is any issue?
Step 1: Pull REF_CTRL low (to GND) and then power on
Step 2: Read all register values (as shown in Image 1)
Step 3: Write in sequence (as shown in Image 2)
Step 4: Measure OUT1(pin11 pin12) to confirm whether there is output.