Tool/software:
Hello,
I'm using the rev B IBIS model to check my 2.5GHz and 200MHz clock quality. I have put 86ohm of termination to ground following the datasheet. My questions are:
1. Is CDCLVP111 output a pull up open drain driver, hence it needs the 86ohm pull down external termination?
2. If #1 is true, can the 86ohm pull down terminate to higher/lower than VEE without causing reliability and back power issue? What is the allowable range of the termination rail for 2.5V-3.8V configuration?
3. Is it expected to have imbalance swing, e.g. the differential cross point to max vs. differential cross point to min has significant delta?
Thanks.