Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: USB2ANY,
Tool/software:
I want to automate programming device with TICSPRO from the command line execution in a batch file using usb2any. The GUI works but I need to automate it for production runs and I do not want to use python or other scripting programs. I can modify TICSPRO.ini file with device and .tcs configuration file (if possible). I would also like the command line to force the EEPROM programming from registers if possible from the same command line prompt.