Part Number: LMK04832
Tool/software:
Hello.
1.) have a single-ended, 10 MHz, analog sine wave coming into our system with an amplitude of 2.0Vpp serving as a master clock.
I wanted to get some thoughts on some signal conditioning needed for this before this feeds to the input of the LMK04832.
If I AC couple this (DC block with a cap) I believe there is some internal biasing on the LMK04832 that will pull the entire signal above ground.
I wanted to ensure that a clean square wave is generated on the output and wanted to get feedback on this.
2.) The datasheet in section 9.1.2.2 describes driving the CLKin pins with a single-ended source. What exactly is the CLKinX_BUF_TYPE doing here?
Thank you for any comments.
Thank you.