This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04806B - max value for Tskew and Td0-delay

Team,

My customer had the below question:

LMK04806B.  On page 18, the datasheet lists a typical value for Tskew and Td0-delay but no maximum value.  I can’t consider this part without knowing the max value for these parameters.  Can someone from the factory specify these numbers?

My apologies in advance if I've posted this to the wrong forum, if so, can you move it to the proper one?

Thanks,

Jim

  • Hello Jim,

    I think we need to pursue this issue with a follow-up call to the customer.  One reason for no max is these specifications are not tested by the ATE test program.

    In the meantime, as relates to Tskew, please note that the number is a typical maximum.  As relates to td0-dleay, please note that there are many adjustment "knobs" which can be used to change the CLKin to CLKoutX delay.

    73,

    Timothy

  • Thanks Timothy - as we discussed, we'll work to schedule a call within the next couple days - thanks, Jim