This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05318B-Q1: Inquiry for Clock Generator IC with Automotive Grade

Part Number: LMK05318B-Q1
Other Parts Discussed in Thread: LMK04832

Tool/software:

Hi Team,

I hope this message finds you well.

We are currently in the process of selecting new clock generator ICs for a new project that should meet the following technical specifications:

  • Number of clock outputs: 10
  • Output signalling type: LVCMOS and/or LVDS, with a preference for low jitter performance
  • Programming interface: I2C and/or SPI
  • Operating voltage: 1.8 V/3.3 V
  • Temperature grade: AEC-Q100 qualified (-40°C to +125°C), preferred to have industrial and MIL grade alternates in the same footprint.


Kindly look into the requirements and recommend the part.

Thank you for your support, and I look forward to your suggestions.

Best regards,
Liston