This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571: LMX2571

Part Number: LMX2571
Other Parts Discussed in Thread: LMX2491, LMX2430

Tool/software:

02-Oct-25

Hello TI,

We are seeking a PLL device to phase lock an external Crystek 1 GHz voltage-controlled SAW oscillator (VCSO) part number CVCSO-914-1000 providing -138 dBc/Hz, 10 kHz offset phase-noise performance for use as a REFCLK source for Analog Devices’ AD9910 DDS synthesizer. 

A 10 MHz REFCLK is preferred, a 100 MHz REFCLK is acceptable.

The AD9910 typical residual phase noise limit is -136 dBm/Hz (10 kHz offset) at the maximum operating frequency of 397.8 MHz. Our testing with a 1 GHz TCXO (-136 dBm/Hz, 10 kHz offset) has demonstrated that the AD9910 can achieve the residual phase noise limit. See the phase noise plot image below. 

Expected temperature operating range: 0˚C to +45˚C

Please recommend a suitable PLL device that can cost effectively support our application.

Thank you. CVCSO-914-1000.pdf