LMK01010: Clock buff, div, dist up to 2 GHz

Part Number: LMK01010
Other Parts Discussed in Thread: LMK04832

Tool/software:

Do you have a part like the LM01010 that can handle up to 2 GHz?

(LMK01010 is limited to 1.6 GHz)

Specifically, we are looking to drive 4 devices (LVDS) at:

2 GHz

1 GHZ

500 MHz

500 MHz

  • Hi Kvin,

    Given that the LMK01010 is such a power-hungry device that cannot meet your frequency needs, you may find success with the LMK04832.

    The LMK04832 is comprised of 2 PLLs (although only using the second one may be ideal for your use case), and can generate up to 13 outputs clocks. It supports LVDS, and could be the perfect use for your case.

    Thanks,

    Michael