Part Number: LMK05318B
Tool/software:
Hello,
The number of registers obtained by the TICSPro GUI is larger than the register map in the "LMK05318B Programmer's Guide". So, my customer has questions as follows.
Q1. Which should I do about registers that are not listed in the Programmer's Guide, #1 or #2 below?
#1 Registers not listed in the Programmer's Guide do not need to be initialized?
#2 Should registers not listed in the Programmer's Guide be written to the data value obtained by the TICSPro GUI?
Q2. All R/W registers listed in the Programmer's Guide should be initialized?
My customer also has questions about Figure 10-1 in the datasheet. (Their “Start-up Sequence" is “EEPROM+SPI(Soft pin Mode)“.)
Q3-1. Initial settings are done in “Device Block Configuration”?
Q3-2. At the initialization, how should the RESET_SW Bit be set? Which is right, #1, #2 or #3 below?
#1 RESET_SW = 1 first. After initializing registers, RESET_SW = 0.
#2 RESET_SW = 0 first. After initializing registers, toggle RESET_SW = 1 to 0. In this case how much time RESET_SW has to be 1 at the minimum before cleared?
#3 If neither #1 nor #2 is correct, Please let them know the right way.
Q3-3. To confirm if PLLs are locked, which register bit should be checked for APLL and DPLL respectively?.
Best regards,
K.Hirano