Other Parts Discussed in Thread: LMX2594, LMX1204
Tool/software:
Hello,
I am using the LMX2594 and my goal is to perform automatic frequency ramping from 1 GHz to 1.7 GHz. However, currently it only ramps from 1 GHz to about 1.237 GHz. I suspect this is due to the channel divider value changing, which causes the ramp to stop prematurely. As a result, I end up getting a ramp range of about 1 GHz to 1.247 GHz instead of the desired range.
To test, I previously tried automatic ramping from 1.795 GHz to 1.890 GHz, and I achieved the expected ramping successfully. In that case, the channel divider value for both frequencies remained the same. However, when I try ramping from 1 GHz to 1.7 GHz, the channel divider value for 1 GHz and 1.7 GHz varies, which I believe is causing the issue.
Could you please guide me on how to properly configure the LMX2594 to achieve automatic ramping from 1 GHz to 1.7 GHz? Any example settings or recommended procedure would be greatly appreciated.

Thank you for your support .