This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5C33414A: VDDO unpowered

Part Number: LMK5C33414A

Hello TI,

May VDDO_2_3 be left unpowered or connected to 0V if / whilst OUT2 and OUT3 are (temporarily) unused? e.g. if OUT2 and OUT3 clock a section of the board which is sometimes powered down?

Put differently, must all VDDO supplies be valid at all times in order to use any OUT clock?

  • Hi Bernhard,

    The datasheet states which supplies must be connected to power because of the internal pins being routed to other internal circuitry.

    Only VDDO_4_7 and VDDO_8_13 can be powered down if unused. The rest must be connected to the supply.

    Regards,

    Jennifer