Part Number: LMK5B33414
Hello, I have some issues configuring my LMK5B33414 with 1PPS Input and output.
My goal is to use the jitter-cleaner function to read the 1PPS input and to integrate it to have a 1PPS output "cleaned" from its natural jitter. How can I manage this ?
I already have a configuration using PLL1 and PLL2 (so only PLL3 is usable) and outputs 0 to 3 and 8 to 13 are already used. I have a input XO of 25MHz (50ppm) and a REF0 input of 48MHz. I want to plug the 1PPS into IN1/REF1 input.
If my configuration is blocking the 1PPS output I can modify it, I just want to have a configuration that allows me a jitter-cleaner function for the 1PPS. A basic example will work just fine.
Please find attached my TICS Pro configuration file that already give me a 1PPS output, but it is not synchronized with the 1PPS input and not jitter-cleaned
Best regards