This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: Phase Noise

Part Number: LMX2595

We need some information about how to improve the Phase Noise of LMX2595 (is there any controlling factors like loop bandwidth etc)

what ever the values given in the datasheet, can we get the same Phase Noise values with Evalution board without doing any changes?

Requirements:

Frequency - 5 to 15GHz, we are not bothering about the settling time.

Phase Noise (@11GHz)- -80 dBc/Hz @ 100 Hz 

                                        -110 dBc/Hz @ 100 KHz