This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B12212: Discrepancy in pin numbering

Part Number: LMK5B12212
Other Parts Discussed in Thread: LMK5B33216

Hello, I have a question regarding the pin numbering for the LMK5B12212. According to the Figure 5-1. in the datasheet the pin numbering for the following pins is:
OUT4_P - 27 
OUT4_N  - 26.

In the table 5-1. the pin numbering is swapped:
OUT4_P - 26 
OUT4_N  - 27.

Could you please tell me which one is correct?

Best Regards
Maciej Trojka
Component Engineer





  • Hi Maciej, 

    Looking at the LMK5B33216 (16-output version of LMK5Bx device) pinout, it looks like it matches the numbering on the LMK5B12212 pin diagram. It seems that LMK5B12212 has a typo in Table 5-1. The correct pin numbering is below:

    OUT4_N  - 26

    OUT4_P - 27 

    I'll bring this up to our team so we can fix this in the next datasheet revision. 

    Regards, 

    Connor