Part Number: SN74LVC1G123
Hello,
I've detected a failure on one cirucit that use the SN74LVC1G123.
The circuit is the one below:

Apparently the timing circuit short the capacitor but don't start the charging phase.
Because the system is a medical device such failure can't be accepted.
In the first images (the working circuit) below on the second trace there is Vc. The behaviour is as described in the datasheet. After a trigger event, the capacitor is shorted and then the charging phase starts. In the second image (the failed circuit) Vc after an initial short can't start to rise.