Part Number: LMK1D1208P
Other Parts Discussed in Thread: CDCLVD1204
Hello Support team,
I have a question regarding to the Specification of the LMK1D1208P Clock Buffer.
In the Date Sheet on Page 6 the Input Voltage is specified as followed
| VIN,DIFF(p-p) Differential input voltage peak-to-peak {2 × (VINP – VINN)} |
| VICM = 1 V (VDD = 1.8 V) 0.3 2.4 VPP VICM = 1.25 V (VDD = 2.5 V/3.3 V) |
| MIN=0.3V MAX=2.4V |
Why is the differential peak-peak Input voltage defined as 2 × (VINP – VINN)?
Isn't the differential peak-peak Input voltage defined as (VINP – VINN)? Where does the factor 2 comes from?
Why I am asking the question is that I want to connect the LVDS DC coupled output of CDCLVD1204 buffer with the DC coupled input of LMK1D1208P buffer.
Would it be possible?
Tank you for your support