This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832-SP: required VCXO specification

Part Number: LMK04832-SP

Hi,

Could you provide the guidance on PLL unlock issue with specific VCXO?

the issue is as below.

  • no issue(CPout 1.4V~2.3V swing) with 603281 from Crystek
  • PLL unlock issue(CPout 3.2V continous output) with MCM8730 from Q-tech

603281 output is 0~3.3V and MCM8730 output is 0.5V~6V.

Please guide what customer set for this issue.

 

Thanks.

 

  • Hi David,

    I cannot find the datasheet of MCM8730. If this device requires a tuning voltage of 3V to get the correct frequency, then you have to use active filter for PLL1. 

    Usually, VCXO requires Vcc/2 as the tuning voltage for the specified frequency. So for a 3.3V VCXO, the tuning voltage is around 1.65V.