Part Number: LMX2615-SP
Hello,
I would like to share the SPI bus for two LMX2615-SP parts with Serial Data Output for readback on the MUXOUT pin. Although the datasheet suggests this is possible by setting MUXOUT_CTRL=0 the default setting for this pin is Lock Detect (output). How can I connect MUXout pins together if they are both configured as output from reset?
Do you have recommendations to prevent damage to both pins while they are mometarily configured as outpus after reset (before they get configured to Tri-State). I considered a series resistor at each pin however I don't know what value to use to minimize damage and still ensure good functionality at the maximum speed of the interface.
| Bit | Default | Desc |
| MUXOUT_LD_SEL | 1 | Lock Detect |
| MUXOUT_CTRL | 1 | Normal Operation |