This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: MCU CLK pin Capcitance

Part Number: TMS320F28335

Hello,

As per datasheet www.ti.com/.../tms320f28335-q1.pdf, page no : 176-177

It is recommended to use an oscillator having the typical specifications as shown below
image.png

We are planning to use a crystal oscillator with a maximum capacitive load driving capability of 15 pF for the external clock. Based on my understanding, the oscillator requires a minimum load capacitance (CL) of 12 pF. Using a 15 pF load is close to the datasheet’s recommended value.

Could you please confirm whether it is advisable to proceed with a 15 pF load, or if a higher value is recommended? Additionally, what margin should be considered to ensure reliable validation?

Thank you in advance