Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595, CODELOADER
We using the LMX2595 in the design of a 4 – 8 GHz synthesizer with 1 kHz steps. We need the spurs to be -60 dBc (mostly) i.e. at a small set of frequencies the spurs can be -50 dBc max.
Our design is trying to utilize the FPD modification to reduce the boundary spurs as suggested by the data sheet, but we are not successful.
Could you please provide some technical assistance in understanding our results below and our interpretation of spurious avoidance?
LMX2595 Boundary Spur Testing
We are working with the LMX2595 evaluation PCB and the TICS Pro software.
Attached are three spectrum analyzer plots and the associated TICS Pro settings.
We are supplying a 100MHz reference source to the evaluation PCB.
1) 7000MHz Spectrum Analyzer Eval Board
7000MHz Settings Eval Board
We set it up to output 7000MHz with only the input doubler activated in the reference chain, i.e. PFD = 200MHz.
Both the phase noise and spurious look good.
2) 7000.1MHz Spectrum Eval Board
7000.1MHz Settings Eval Board
We then offset the frequency by 100KHz, with all other settings except the NUM=1 being the same.
This produced serious spurious components in the spectrum. We understood and expected this to be boundary spurious as
7000.100MHz Mod 200MHz = 100KHz
3) 7000.1MHz Spectrum Analyzer 240 Ref Eval Board
7000.1MHz Settings 240Ref Eval Board
Our intent in production is to deal with the boundary conditions by changing the input reference chain as discussed in the data sheet.
We changed the PFD to be 240MHz by setting the input doubler = 2, PreR = 5, Multiplier = 6
We adjusted N=58, NUM=1435234903, and DEN=4294967291 to achieve 7000.100MHz output.
In this case 7000.100MHz Mod 240MHz = 40.100MHz which is quite far outside the boundary condition of the loop filter. However, we still see the same poor spurious performance.
We did also review your technical note snaa289 and downloaded the CodeLoader software. However, the LMX2595 is not supported by CodeLoader.
I look forward to your response.
Best regards,
Richard Scheer