This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04031: What is the phase delay if the part is in bypass mode (output frequency is equial to input frequency)?

Part Number: LMK04031

Hi TI,

What is the phase delay if the part is in bypass mode (output frequency is equial to input frequency)? And is the duty cycle almost 50:50 in bypass mode as well? Any extra limit for that bypass mode? Thanks!