Part Number: LMKDB1202
Hello, I see that the LMKDB1202 has separate supply pins for both the clock inputs as well as separate bank supplies for the output buffers. I am wondering, is it possible to operate the component with partial / separate supplies depending on the use case?
For example, if CLKIN0 and CLKIN1 come from different clock sources in different power domains, if SEL is such that CLKIN0 is routed to the outputs can VDD_IN0 be powered by CLKIN0 source and VDD_IN1 be powered down while CLKIN1 is unused and also powered down? Basically if VDD_IN are shared with the oscillator power sources in a partial power down / cold spare situation.
Similarly for the output buffers / banks. If one of the two outputs is permanently unused and OE# tied high, can that output bank be powered down?
Thanks.