Part Number: LMK01801
Other Parts Discussed in Thread: USB2ANY, USB2ANY-UWIRE,
Hi,
In the Pin Control Mode, what is the mechanism of setting for Middle?
Could you something elaborate explanation about it?
According to LMK01801 User’s Guide (SNAU118A – December 2011 – Revised February 2018),
"Headr = Middle" on Table 2 is shown header-pins 3-4 shorted on the schematic.
And it connected to ground via a 27kohm resistor(weak pulldown?).
On the other Hand, "Headr = Low" is header-pins 5-6 shorted to GND directly.
"Headr = High" is header-pins 1-2 shorted to VCC directly.
Are there any voltage-dividing resistors inside the device?
Regards