Part Number: CDCV304-EP
Hello,
I would like to know what's the min, typ, and max duty cycle for this part number. My input clock signal works at a 40% duty cycle signal, and I would like to know if it can be supported.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCV304-EP
Hello,
I would like to know what's the min, typ, and max duty cycle for this part number. My input clock signal works at a 40% duty cycle signal, and I would like to know if it can be supported.
Hi Natalia,
The same applies for this part as the thread you linked.
The output duty cycle should be close to 50% assuming a input clock with a 50% duty cycle.
This is a buffer though, if your input has a 40% duty cycle the output should have a 40% duty cycle as well.
We do not have this spec'd though as all applications usually will have a 50% duty cycle input as well as 50% duty cycle output.
Best regards,
Vicente