Part Number: LMX1214
I configured the LMX1214 registers using TICS Pro, but there are discrepancies with the datasheet.
(1) R8 Register AUXCLKOUT_EN: In the datasheet, it's assigned to D5, but in TICS Pro, it seems to be assigned to D4.
Which is correct, the datasheet or TICS Pro?

(2) In the TICS Pro GUI below, checking the MUXOUT checkbox sets D6 of R23 Register to '1', but in the datasheet, it's '0', and it appears nothing is assigned. Is it necessary to set R23 D6 bit to '1' when using MUXOUT?