Part Number: LMK05318B
We see a reference to the ability to set one of the LMK05318B outputs to 1 Hz and then synchronize that with an external source. Is there any more information available about how to implement this?
We are using PRIREF for the primary clock input (about 8 MHz) and would like to program one of the outputs to 1 Hz and then synchronize that with the PPS signal from a GNSS receiver module. Could that be applied on SECREF, or would we need to move the primary clock to SECREF to apply the PPS sync input to PRIREF? Or do we misunderstand how this works?
Also, if one does synchronize this way, what is the delay or uncertainty range? In other words, after sync how closely will the 1 Hz output be aligned to the sync source?
Thanks!