Part Number: MSP430FR6007
Hello,
I´v got some questions regarding forwarding the MSP430 ACLK on P9.3 to an external device.
Conditions:
- ACLK is sourced by dig. ext. 32.768kHz oscillator on LFXIN
- ACLK is output on P9.3 continously over whole lifetime
- lifetime is 12 to 16 years
- operating temperature: -20°C to +75°C
Questions:
- what is the max. load capacitance the output can drive? Within the datasheet the electrical specifications are measured @ 20pF
- is the output stable over the full lifetime? are there any experiences regarding this?
- what is the current consumption with the output active? Cload * f * VDD?
Thank you and best regards
Philip