Part Number: LMK04828-EP
Other Parts Discussed in Thread: LMK04828,
The LMK04828 data sheet states a power down supply current of only 1-3mA. But to me it's not clear how this mode actually can be entered - at least in the TICS Pro power calculation setting the 'powerdown' flag (under Mode Control) won't make any difference in total consumption.
Or is this just a bug in TICS ?
- What has to be done in order to achieve this 'power down' supply current of only 1-3mA ?
- Is just setting the 'power down' bit (bit 0 @ reg.2) sufficient ?
- Or do additional power down bits of the different internal components (like mux, PLL, divider, etc) have to be set in addition ?
- Can an external TCXO, connected to OSC_IN+/- still run during LMK power down mode or should it be disbled too?
- At least in TICS Pro it's never possible to achieve such a low consumption - even if everything has been disabled or set to power_down - is this a TICS bug?
Thank you for your help!
Markus