This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCBT1001: CDCBT1001 Application for 50ohm termination load

Part Number: CDCBT1001

Hi TI team,

We are using CDCBT1001 with VDD_OUT = 2.5V to drive a single-ended 10MHz clock at 50ohm load as picture below. Vout is (2.5)(34)/(34+50)=1.5V due to voltage divider and Iout is 2.5V/(34+50)=30mA which is below maximum continuous output current 50mA, but since datasheet does not list out the recommended operating condition for VDD_OUT=2.5V, we would like to know if this 30mA would cause damage to the device and shorten the device lifetime or it is acceptable for the device under this kind of operating conditon? BTW, Is there other recommended buffer IC that is able to drive a 50ohm load under recommended operating condition...?

 driver.jpg

Thanks,

YW