Part Number: LMX2492
Other Parts Discussed in Thread: LMX2491
Hello,
I would like to use the LMX2492 in a special ramping application. Essentially, I need to be able to increase the start frequency by a fixed step size after every ramp. The bandwidth of each ramp is identical. The time between ramps is very short, only a few microseconds so I would like to avoid reprogramming via SPI between ramps. Is this possible by simply having an up profile and a down profile that doesnt return fully to the starting position? Are there limitations? What would be the recommended approach for this?
Also, I was wondering how the external triggers from GPIOs operate. Are they sampled using the PFD clock? Are there any specifications to their setup and hold times? Thanks!
best regards
Dominik