Part Number: TLC555
Hi team,
My customer wants to use TLC555 to generate PWM signal with 500Hz freq and 50% duty cycle. The supply voltage is 5V and no external trigger. How to set the component is suitable?
Regards,
Eileen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLC555
Hi team,
My customer wants to use TLC555 to generate PWM signal with 500Hz freq and 50% duty cycle. The supply voltage is 5V and no external trigger. How to set the component is suitable?
Regards,
Eileen
Hello Eileen,
RA = 10k
RB = 133k
RD = 301 ohms
C = 10nF

Variance from full tolerance range.

Hi Ron,
Thank you for your reply. If the freq is 400Hz, how to set them? The customer needs another PWM signal with 400Hz freq and 50% duty cycle, the other condition is the same.
Regards,
Eileen
Hi Ron,
What the precision requirements for the components? Are they listed in the first column of the table? If so, 0.1% tolerance resistors are not available in the customer's component library. Can they replace RB with 1% tolerance one?
Regards,
Eileen
Eileen,
I have no requirements for precision. The main point of the table was to convey the point that output is about 500Hz and 50%
1% resistors are fine. RB being 0.1% in table is point out that it is the most important resistor (of the three).
The 5% for cap is to point that the capacitor is the main cause of output variance. It's tolerance, voltage and temperature modulations.
Eileen,
The full FAQ is here: [FAQ] How do I design a-stable timer, oscillator, circuits using LMC555, TLC555, LM555, NA555, NE555, SA555, or SE555?
Frequency is inverse to resistors. They could factor the resistors by 500/400 = 1.25 the previous value
RA 12.5k (12.4k) , Rb = 166.25k (165k), Rd = 376 (374 ohms)
Hi Ron,
Thank you for your reply. I'd like to confirm that, for 400Hz output, can we keep the RA=10K, but change RB to 174K?
Regards,
Eileen