Part Number: CDCEL937
Other Parts Discussed in Thread: CLOCKPRO,
We are using the CDCEL937PWR as a baud rate generator for RS422 communication. It has 9 outputs but I only need 6. Our design consultant has chosen either a 100MHz or a 29.49MHz clock as the input frequency. Unfortunately if one of these two is chosen it cannot be changed. I have downloaded the ClockPro software and I am having trouble acheving the baud rates that I require.
Here are the baud rates (yes, they are slow):
1200, 2400, 4800, 9600, 19200, 38400, 57600, 115200
Can they be obtained with the CDCEL937PWR?