Part Number: LMK04832
Hi,
On my board, LMK04832 has CLKIN0 connected to the 3.84 MHz , and CLKIN1 connected to the 245.76 MHz from the previous PLL. OSCIN is left unused. I want to output clocks in single PLL2 mode or Distribution mode. However, no clock frequency can be detected on any output pins regardless of configuration settings.
All register read/write operations of the host controller for the LMK04832 are configured correctly. The input clock signals and reset signals are also working normally.
Please help check my configuration file, the attachment file.
LMK04832#1-SINGLE-PLL2.zip LMK04832#1-Distribution.zip