Other Parts Discussed in Thread: CDCE72010
Hi,
I have another post on syncing multiple CDCE72010's across a system but this question is a little different so I'll put it in a new thread.
My clcok input is through the VCXO pin. I am not using PLL's or VCO, ect. I just run straight off the clock and use the dividers for each output.
If I want to sync to an external signal I set reg6 bit 5 and use the reset input. The only problem is I don't see any spec for reset with respect to the VCXO input clock that can help me determine the timing required to obtain sync on any particular clock edge, or even if it's the rising or falling edge. It is very important to our system to sync properly to a common clock edge.
The only spec I see on reset (and powerdown) is max 4ns risetime.
Thanks.