Part Number: LMX2572
Two LMX2572s share a 100 MHz OSCin (one integer-N, one frac-N, 500 kHz offset), hopping 5 MHz steps every 30 µs with FCAL_EN=0 (pre-characterised VCO_SEL), FastLock, VCO_PHASE_SYNC_EN=1, SYNC pulsed at every step.
- Datasheet §7.3.11 includes "analog settling time of the PLL loop" in t1 — may SYNC be asserted at a fixed delay after the R0 write, before the loop has settled, with synchronization completing once it settles?
- If the loop slips a cycle after the SYNC pulse is latched, is output phase determinism preserved?
- If the channel divider is already in the correct state, does a SYNC pulse produce any output phase perturbation, or is it a true no-op?
- With MASH reset on every R0 write, what MASH_RST_COUNT constraint applies at a 30 µs step period?